Hi,
I have a some questions realted to using TPS7H5001-SP in a Push Pull converter:
1) Figure 9-1 in the datasheet, the SR GaN FETs are driven with respect to GND to avoid using BOOTstrap effect in GaN driver ?
2) this will lead for the output to be taken from Transformer CT after LC/LC filter, correct ?
normally the two terminal of the Transformer should go through a switch and their outpts are joined together to LC filter where output is taken having CT used as GND.
3) if we need to add another SEC winding that produce excatly the same voltage but with a negative sign, how should the other winding Schemtic looks like ?
Thanks!
Mohamed