Other Parts Discussed in Thread: UCC28951
Hello,
I want to use a UCC28951 to design a 390V to 40V power supply. I'm using your SLU222E file to calculate the parameters and components. In my case, the output power can range from 30W to 800W. I want the current in the output inductor to never drop to 0A and remain within the continuous operating range, even at 30W. To achieve this, I would need to be able to directly control certain "white" cells in the spreadsheet, such as the IL out delta. Would it be possible to obtain the code to unlock these cells? Thanks in advance.
Rafael Leroy