Other Parts Discussed in Thread: LM74910H-Q1
Hi,
it seems that i do have aproblem with undrestanding of the SOA. i am looking for MOSFET for my ORing IC (LM74910H-Q1).
assumptions: 6A, Vmax=34V, VGS=10V, @100°C: RDS-ON = 1.45*0.79mOhm=1.1mOhm
my selection process is:
1- VDS = 6A*RDS-on = 6A*1.1mOhm = 6.6mV
2- look at figure 10 of the datasheet. extending the RDS-ON limit line (gray) to VDS=7mV -> it can handle about 4A continuous at 7mV drain-source voltage.

is my method wrong? considering the 1.1mOhm, the power losses of the MOSFET is about 40mW (1.1mOhm*6A^2) which is not a problem. Do i consider wrong VDS for my calculations/selection?
BR Toktam