Hello,
I am currently designing a buck converter that is going to be used in our Formula Student vehicle. I think that the LM5176 is a giid choise as it includes features such as high Vin range and Iout. To ensure that the design will run as expected i have run the simulation that you provide in pspice with gust changing Vin and the feedback voltage divider (I want Vout = 24V and i have used R1 = 280k, R2 = 10k ). The problem is that is the simulation Vout reaches max 21.5V, is this a simulation problem or am i doing something wrong.
Thanks for your time.