Hello TI Support Team,
I am designing a backlight driver for a display that requires approximately 27 V @ 280 mA.
The desired input voltage range in my system was 5 V to 40 V. After reviewing several options, I found that the LP8868V-Q1 is suitable for my application. From the datasheet, I understand that the LED backlight is referenced to the input voltage, not the ground. Based on this, I designed a backlight driver to operate from 5 V to 36 V, with the OVP pin set to 63 V.
Design Parameters:
- Input voltage: 5 V – 36 V
- Typical output current (maximum brightness): 280 mA
- Maximum designed output current: 500 mA
- Switching frequency: 600 kHz
- PWM dimming, with reserved components in case I decide to switch dimming methods after testing
- Compensation network values follow the recommended design from the datasheet as a starting point; I amm currently deriving the transfer function and Bode plot for further verification.
The schematic is attached below.
Could you please review it and suggest any enhancements or improvements to help avoid potential issues before proceeding with manufacturing? If possible, I can also share the PCB layout privately for your review.
Thank you for your time and support.
Best regards,
Malek