Part Number: UCC5350
Other Parts Discussed in Thread: UCC21550,
Hi,
Could you recommend the device for below requirement?
1) Working voltage : 900V
2) Fsw : 100~150kHz
3) Device : 1200V SiC MOSFET
4) Topology : Half bridge
There are 2 consideration with UCC5350 and UCC21550.
Please check best fit device and check the availability of below considerations.
UCC5350: use 2 units with 2 supplies and add dead time circuit at high side and low side input. will use the dead time in both of DSP and driver.
UCC21550: 2 power supplies. for example, 18VA, -3VA@VDDA, VSSA. 18VB, -3VB@VDDB, VSSB