Other Parts Discussed in Thread: UC2854, UC1854
Hi
I am using UC2854 for 115V, 360Hz to 30V convertion for 15W power supply, For room temperature gate pulse starting at 2nd negative cycle itself, but while testing at 110deg the pulse starting at 3rd negative half cucle only. I am starting from zero deg phase only for all temperature. I need to meet 12ms startup time, I can't meet at high temperature due to this switching delay, In datasheet there is no information about this delay.