Part Number: LM51561-Q1
Hello!
On my last post (https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1521807/lm5156-q1-sepic-converter---mosfet-overheating/5850758) I shared an issue I had with a SEPIC topology using the LM51561-Q1 on which the MOSFET was overheating beyond what was expected.
When we tried a MOSFET with smaller gate capacitance the result was better, even though the on Resistance was bigger. At the time I reached the conclusion that the bigger capacitance on the gate was making the turn-on time too slow, and the MOSFET was overheating because of that.
Now, we were able to test other MOSFETs and the results are shown below:

- BUK7Y7R8 (Original)
- BUK7M17-80EX (Last Post substitute)
- PSMN041-80YL (New)
- BUK7Y38-100E (New)

Yet again, the best performing MOSFET was the one with the smaller capacitance.
We noticed that the inductor is also overheating, even though it is rated for 5.23A rms and we are using a 2A load, so we decided to investigate further.
The picture below shows the waveforms for a 2A load:

Yellow - MOSFET Drain
Purple - MOSFET Source
Blue - MOSFET Gate
Green - Diode Anode
We believe this oscillation on the MOSFET drain is the main reason the MOSFET and inductor are overheating. We tried adding gate resistance, but if we slow it down too much, it also overheats because it stays too long on the linear region.
Do you think this oscillation may be the reason for the overheating issue? Can a snubber across Vds solve it? or should it be from Vd to GND? Also, how does it relate to the MOSFETs we tested and the temperature results? is it really a gate capacitance issue?
Thank you in advance.
Wagner M.