Other Parts Discussed in Thread: ADS1115, LM2776, LM7705
Hello IT experts,
I am using the INA823 in a simple power configuration (+Vs = +5 V, –Vs = GND) to measure 0–10 V and 0–20 mA analog signals.
When the input is 10V or 20mA, the output is about 2V, which is correct.
However, when the input is 0 V (or 0 mA), the output does not drop completely to 0 V, but instead remains around 9 mV, which affects the reading on the ADS1115 ADC.
By applying a small negative supply (–5 V) to the Vs– pin, the output offset decreases considerably to about 168 µV.
- Is this residual voltage (~9 mV) normal behavior when operating with +5 V supply only?
- Is it necessary to use a negative rail (e.g. with the LM2776) to get accurate readings close to 0V at the output, or is there some recommended configuration to achieve true 0V in single supply mode?
Thank you in advance for your support.
Best regards,