This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2400: Protection IC alternative to TPS2400

Part Number: TPS2400

Hello team,

My customer is looking for a overvoltage, undervoltage, reverse protection component. They were looking into the TPS2400 but that does not suffice in terms.

Do we have a component with the following specs?

  • OV threshold (rising) = 5.54 ... 5.71V
  • UV lockout: 2.95 ... 3.05V
  • Turn-off delay: max 4 micro sec.

and another component with:

  • OV threshold (rising) = 3.56 ... 3.67V
  • UV lockout: 1.96 ... 2.02V
  • Turn-off delay: max 4 micro sec.

 

Thank you.

Kind regards,

Wouter Kragt