This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS552882-Q1: Power dissipation calculation

Part Number: TPS552882-Q1
Other Parts Discussed in Thread: TPS55288

How to calculate the dissipation on TPS552882QRPMRQ1 IC and the two external N channel Mosfets for the following use case

1) Input 8V/24V and Output 12V @7.5A

When estimating dissipation based on efficiency, the calculated loss is around 10 W, which seems quite high.


Clarification is needed on whether this value is realistic and if the device can reliably operate at an ambient temperature of 85 °C under these conditions.

Thanks