Other Parts Discussed in Thread: UCC21710
Hi All,
We are trying to use the UCC21710 and we are having an overcurrent shutdown on our LS FET Driver. We have tried floating it and pulling it down with a 3k. No luck. We tried completely shorting the pins and still faulted. We have been unable to successfully stop the LS from faulting and replaced the chip as well as supporting circuitry. Attached is a schematic. We are not using the Temp sensor currently either. We are trying to drive the AIMCQ120R030M1T, a 1200V SiC FET. It is being powered by the UCC15241, and these voltages function without issues.