Part Number: UCC28180
Other Parts Discussed in Thread: UCC28951, , UCC27714EVM-551
Hi,
I am creating a AC/DC power supply module taking in line voltage 230Vac A 50/60Hz and outputting 48Vdc/10A continuous. The high level architecture is "Line input (with some protection and EMI filtering) -> Power Factor Correction circuit (UCC28180) -> Phase-Shifted Full Bridge circuit (UCC28951) -> Output".
I do not have the schematics done yet, but I have based my design on UCC28180EVM-573 and UCC27714EVM-551 (this EVM uses UCC28951). I have attached both EVM pdf files. Inside those files at the EVM schematic page, you will find the EVM schematics with annotations on the components that we have selected to meet our design requirements. The selection of components is supported by "UCC28180 Design Calculator Tool: SLUC506" and "UCC28951 Excel Design Tool: SLUC222E" which I have also attached.
I would like to request your assistance in reviewing the excel design calculators and our selection of components and feedback if you noticed any issues or any blind spots that we may have missed. The schematics that we want will largely reference the EVM.
I have also attached a "Design Requirement" word file that summarizes all the design requirements that we are trying to meet. If additional information is needed, feel free to ask!
Design Requirements.docx SLUC222E_10A.xlsx [User's Guide] sluub02a.pdf sluc506c_10A.xls [User's Guide] sluuat3b.pdf