This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS552882-Q1: TPS552882QWRPMRQ1 Output Voltage Instability

Part Number: TPS552882-Q1


Hello Team,

We are using the TPS552882QWRPMRQ1 buck-boost regulator in our design. The input voltage range is 3.3V to 4.2V, and the expected output is 3.8V at 3A.

However, we are observing instability at the output when powering on the device — the output voltage varies, and in some cases, we are getting a constant 4.8V instead of 3.8V.

Could you please help us analyze and resolve this issue?

Regards,

Amit