This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM22678: need a Negative power stage.

Part Number: LM22678
Other Parts Discussed in Thread: LMR36506, LMR51606

hi Sir

We need a Negative rail stage. Vin:24v, Vout -15v/200mA

LM22678 Is suit? thanks

did you have any guide to do the DC inveter?

thanks

  • Hi,

    LM22678 is a 42V device and 24V to -15V comes out to be 39V across the device. It is not recommended to use with such a low margin and is better to go for a 60V device.

    If 200 mA is the max current, you can consider LMR51606 or LMR36506

    You can refer this app-note for inverting buck-boost implementation : www.ti.com/.../snva856b.pdf

    Regards,

    Niranjan