Other Parts Discussed in Thread: TL5001A, TL5001, TPS40200, TPS40210, UC28023
Hi:
I'd like to use the TL5001a for a VM boost controller running at 500kHz, I need around a 65% duty cycle max. Can this part do that?
The datasheet doesn't seem to list a min off-time. Also, the written notes say it can go up to 500kHz, but the Rt figure (fig 5) only goes to 400kHz. Plus I've seen a TI tech note that says it can only go to 400kHz.
So can it go to 500kHz? If so, what Rt is required? 10k?
Please help clear this up for me.
Thanks.
p.s. If this part can't do 500kHz at 65% DC, can you recommend another low cost VM controller that can? FYI, my app operates at 10V to 14V.