This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: LM5176 output voltage during FB circuit failure

Part Number: LM5176
Other Parts Discussed in Thread: LM51770, LM51772

If the LM5176's FB pin fails and is pulled to GND,
it will likely continue to boost the output voltage.
I would like to confirm the output voltage at that time.

Input: 12V
Output: 12.8V (RFB1: 20k, RFB2: 300k, L1: 5.6uF, RT: 23.2k)

image.png

1. To what voltage will the output voltage rise?
1. Is this the result of some kind of protection function?

Thank you in advance.