This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25940: VIN=22.2V in 2us

Part Number: TPS25940

Hi team,

During customer prototype evaluation, there is a possibility that an inrush voltage of approximately 22.2V (for about 2us) may be input to the IN pin, which exceeds the ABS MAX input voltage rating (20V) The datasheet also mention up to 22V (for 10ms) is tolerated. Can 2us 22.2V be accpetable? 

If the above situation should be avoided, could you please suggest another eFuse with similar spec but with an ABS MAX rating of around 30V?

Best regards,

Hayashi