Hi,
We use the TPS5430DDAR for the DC/DC design, the input is +15V and output is -15V, now, we order the new TPS5430DDAR which the silk screen is include the TI logo and PIN#1 point but remove the Pin#1 line, and the output voltage rising edge has the voltage overshoot, please refer to below schematic diagram and waveform and check if there are any design modification between the new silk screen and old silk screen, thanks.