Part Number: TPS54531
Dear Sir & Madam,
As per your suggestion, I have drawn the schematic using the TPS54531 IC. I am facing the following issues during testing:
-
When the input voltage is between 12 V and 13.8 V, noise is coming from the inductor. And Inductor also slightly Heating, However, when the input voltage increases above 14 V up to 27 V, the noise disappears.
-
When I connect the load (a charging IC for 2-cell Li-Po Battery, 3.7V/2600mAh, Model 18650), a short occurs at the output side of the Capacitor C65,C66 .
My input voltage range is 12–27 V, and the required output is 12 V / 4.5 A. and This my Inductor PartNumber ASPI-0630LR-100
I have attached the schematic for your references.
Kindly review it and advise on possible causes and solutions for these issues.TPS54531-Power_supply.pdf
Best regards,
P.Mahesh