Hi All,
I have a question about the LM51772.
A customer is evaluating the device with VIN=24V, VOUT=5-48V, and IOUT=2A (max).
VOUT is set via an I2C register.
(1) When VOUT is set to 5V, it initially sets to 5V, but then slowly rises.
It rises to 55V. This occurs when there is no load.
VOUT stabilizes when a certain load (1mA) is applied. What are the possible causes?
(2) In the above condition (1), when a load current of about 1A is applied, VOUT down to 4.5V.
When VOUT is checked with an oscilloscope, it is oscillating.
At the same time, Vcc2 is also oscillating, which seems to be affecting it. What are the possible causes?
I have the circuit diagram and register settings, so I can share them via private message.
Best Regards,
Ishiwata