BQ25172: TS pin as Enable/Disable

Part Number: BQ25172


Hi team,

I would like to use TS pin as to control charge enable/disable via MCU GPIO.

It seems that we should pull down to GND for charge disable.
On the other hand, what should do for charge enable? Floating is acceptable?

If you have the reffrene circuit for this usecase, it would be very helpfull.

Best reagards,
Goto

  • Hi Goto

    It seems that we should pull down to GND for charge disable.
    On the other hand, what should do for charge enable? Floating is acceptable?

    Yes, pull down to GND will disable charge, floating will enable charge.  BUT during floating the TS pin is monitoring NTC for temp and the current source is only 35uA.  The GPIO in floating condition needs to be high impedance for accurate temp monitoring.

  • Hi Bill,

    Thank you for comment.
    Let me add a bit more. In this case, we do not monitor the temperature.
    We would like to use TS as only Enable/Disable.
    Can we control charge Enable/Disable by switching the Hi-Z/Low output of the GPIO in the following configuration?

    Best regards,
    Goto

  • Hello Goto,

    What is the value of Rpd? As Bill mentioned anything connected to the TS node needs to be high impedance otherwise it will impact the temperature measurement.

    Sincerely,

    Wyatt Keller

  • Hi Goto

    We would like to use TS as only Enable/Disable.

    If NTC is not used then need a 10k pull down on (Rpd).  This will keep TS voltage at about 350mV - safe range is 188mv to 1.04V.  

    The GPIO needs to be low enough to keep unit in safe range.