Dear TI experts,
My customer asked buck converter under the condition below.
Vin=5V
Vout=0.5V
Iout=1A
AEC-Q100 is required.
Actually I suggested TPS62921-Q1 based on WEBENCH simulation.
But it simulated as 0.4V output although I input 0.5V output.
And as you see Rset is 4.87Kohm.

It is just the same as the datasheet.

So my question is,
Can't TPS629210-Q1 make 0.5V outout using the value between 4.87K and 6.04K?
If it can't, could you recommend buck converter which can make 0.5V/1A output?
Vin is 5V.
Best regards,
Chase