This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A88: TPS7A8801RTJR - Simulation Query

Part Number: TPS7A88


Hi Team, 

Is there any tool available that supports power simulation for this IC?

Regards,
Vinay

  • Hi Vinay,

    We do have a PSpice model available for this device that models basic transient performance of the LDO, including voltage drop and input current. That model could be used for a basic power analysis. The basic model doesn't model the error amplifier bandwidth or device output impedance, so load transient results may not be identical to the physical device.

    Best Regards,

    Alex Davis

  • Hi Alex,

    I have completed designing the LDO regulator. Please find the attached regulator section for review and also please let me know if anything needs to be changed w.r.to design 
    Part Number: TPS7A8801RTJR

    LDO_REGULATOR_DESIGN.pdf

    Regards,
    Vinay

  • Hi Vinay,

    With 3.3V in and 1A of load on both the 1.2V and 1.8V outputs, power dissipation in this design will be 3.6W, and may cause the design to exceed the recommended 125°C junction temperature at ambient temperatures above around 6°C. 

    If 1A output is required on both 1.2V and 1.8V outputs and no lower-voltage supply is available for the input in your design, I'd suggest using two separate LDOs to help split the power dissipation up and reduce operating temperature.

    Best Regards,

    Alex Davis

  • Hi Alex,

    The 1.8V OUT1 rail requires 100mA, and the 1.2V OUT2 rail requires approximately 688mA.
    Should separate LDOs be used for these two voltage rails considering their respective output current requirements?


    Regards,
    Vinay

  • Hi Vinay,

    With the reduced output current in your application, this should be okay. Using the 33°C/W RθJA value from the datasheet, the junction temperature should remain within the recommended range up to an ambient temperature of around 72°C with these load currents. 

    Best Regards,

    Alex Davis