Part Number: TPS25946
Does Figure 7-13 in the TPS25946 data sheet SLVSGA8B show the current limit accuracy below 1A? From the graph it looks like at 500 mA the accuracy is between -15% to +15%. Is this correct?
If I cannot use Figure 7-13 for the current limit accuracy, what accuracy can I expect for the current limit at 500 mA?