This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951: how to configure delay time for UCC28951?

Part Number: UCC28951

Dear PL AE

my customer design in UCC28951 in their project and they have several issues as below associated with datasheet of UCC28951 need consult.

  1. in figure simplified appliaction(page 1),  figure 7-18(page 35), 8-3(page 40), the ADEL pin connected to CS pin by RAHI. this meets all descriptive in the datasheet. but in figure 8-5(page 56), seems ADEL pin actually connected to VREF. is this correct and what is the reason?
  2. in page 46, what is part number for infineon's MOSFET? I checked IPP65R190CFD and several Infineon's 650V/20A CoolMOSFET. the output capacitance is in range 23~100pF and measured in 400V or 100V. the datasheet said the output capacitance is 780pF@25V. also, there has several output capacitance such as time related capacitance, energy related capacitance. so my question is: which cpacitance should be used to calculate tank frequency in Equation 89?
  3. Does TI has any document to explain equation 49 & 80?
  4. Does TI has any document to explain equation 90(page 52)? also, seems the equation 90 and equation 131(page 60) is not exactly same. which should I used to decide the delay time?
  5. in equation 134(page 61), what is voltage of CS? the KA=0.0405, according equation 134, I can deduce that voltage of CS=3.461V. this is over CS range: 0~2V. Do I have any mistake or misunderstanding?
  6. for equation 143(page 65), in my application, output voltage is vary from 0~500V. how should I calculate Me and then Rsum, RDCHMI? 

big thanks for your supporting.

regards,

Bill