TPS62065-Q1: Power Section Schematic Review

Part Number: TPS62065-Q1


Creating a PCB for Car Geofencing. I'm specifically using automotive-grade IC(Q1). This is my power section that I have decided to use.

  1. Please help me with the best layout practice for these power sections.

  2. Also, important points(clearance and creepage) to be considered when using wireless communication modules like Quectel, MAX10S GPS, and BLE Modules on other side of PCB.

  3. Other suggestions besides this are welcomed with open hands.

Input: 12V battery input(lead acid mostly) and additionally needed reverse voltage protection and transient voltage prot in 1st prototype.