Part Number: TPS7H5001-SP
Hi,
for the flyback calculator, I found some formulas that seem not correctly subsituted.
row 81: RfBU should be RCOMP not RBOTTOM, correct ?
row 82: Gcs is subsituted as 3, GCS should be RCS/g_cssp which is row63/row52, correct ?
row 83: FZESR should be row 79 not RHPY in row 58, correct ?
row 84: excel formula not correct needs update and removing 3 and putting turns ratio, correct ?
after I did all these edits in Simplis I got really poor performance in terms of PM & cycle by cycle current limitng. the funny part is when I keep the compensation values in the flyback referecne design as on your website, it seems to work well.
this seems like a contrdiction between the Book1.xlsx analytical values and the simulation results.
would you investigate that and let me know the outcome please ?
I tried to add the schemtaic but it is not possible, I can surly share it if there is a way to do that.
Thanks!
Mohamed