Other Parts Discussed in Thread: CSD95490Q5MC, CSD95410RRB, CSD96497Q5MC
Dear TI Team,
I am planning to use TPS53667 + power stage solution in my design for the generating the below requirements. I have seen the CSD95490Q5MC recommend to use in the TPS53667 datasheet and EVM. But CSD95490Q5MC is showing NRND in TI site and CSD95410RRB is showing as the alternate part. But this part is currently under NDA and the sales team updated me that they cant proceed with the creation of NDA now as they dont have anyone covering our company.
Could you please suggest an alternate power stage and also please share how many power stages required in our design to meet the requirements?
Desing requirements:
Input voltage: 12V
Output voltage: 0.75V +/-5%
Output current: 40A DC RMS, 60A PEAK
Product EOL: 2030
Thanks in advance.
Regards
Shyam