Part Number: TPS5430
I'm using a TPS5430 IC for 12-5V Power converter. The issue is the circuit fails in EMI/EMC testing, at multiple points.
I'm attaching the schematic and layout below. I followed the recommended layout as much as possible. Thing is the circuit fails in Radiated EMI emissions test.
I'm using a shielded inductor, poured ground around the buck converter and in the layers below as well.
1. Need support from the TI Experts to solve the emissions issue
2. The recommended layout in the TI datasheet has a huge switching node with a very large area is it okay? while the app note also contradicts saying the switching node should be as low possible. which one to follow?
3. should we pour ground underneath the inductor?
A couple of things that I'm thinking to do to solve this is:
1. Add bulk capacitor in the input
2. Replace ferrite bead in the input with a inductor.
Apart from this it would be helpful if you can help me in fixing this!
Thanks!