This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63070: Regarding the Overvoltage Protection Threshold

Part Number: TPS63070


Hi team,

My customer is considering the TPS63070 based on the following requirements:

Requirements:

  • Input voltage range: 2–9V

  • Output voltage: 5.5V

  • Output current: 0.8A

  • Topology: Buck-Boost

With a lower input limit of 2V, the number of suitable devices is limited, and the TPS63070 seems to be one of the few viable options.

Question: According to section 8.4.8 "Overvoltage Protection" in the datasheet, it appears that the threshold is internally defined. What is the exact value? The customer would prefer a threshold around 6V, but this cannot be configured by the user, correct?

Best regards,

Kyohei