Part Number: CSD18540Q5B
Other Parts Discussed in Thread: CSD18512Q5B, LM5145, CSD18534Q5A, CSD18531Q5A
Hello,
I am working on making a solution that uses the CSD18540Q5B. After running my calculations I've noticed that when using the typical parameters my design will not overheat. However, when using only the worst case parameters, the design comes close to overheating.
I'm curious where variation occurs. For example, if I order a reel of 1000, how much will the operating parameters change in that set of 1000? And then, if I order another reel of 1000 half a year later, is the variation from Lot A to Lot B much greater than the overall variation of Lot A?
If the majority of variation occurs chip-to-chip, we can then do testing to remove the boards that overheat and end up with a percentage that passes. However, if the majority of variation occurs lot-to-lot, we could end up with 1000 boards that don't work.