This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULN2003A: In the ULN2003A Figure 5-5, does the maximum collector current graph show the value per channel?

Part Number: ULN2003A

1. In the ULN2003A Figure 5-5, does the maximum collector current graph show the value per channel? (For example, when N=4, 70°C, and DUTY=100%, the maximum value per channel is approximately 57mA. 57mA x 4 = 228mA in total.) 2. The absolute maximum rating: The maximum for each channel is 500mA, and the maximum for the total is 2.5A. Is this correct?