This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63700: ±15V/500mA DCDC

Part Number: TPS63700
Other Parts Discussed in Thread: LMR60410, TPSM33615

Hi,

Could you please let me know the products with low price and small package size that satisfy the following conditions?

-VIN=24V, VOUT=15V, IOUT=500mA
-VIN=24V, VOUT=-15V, IOUT=500mA

Is there any product that can output -15 V with built-in inductor DCDC?

Best Regards,

Nishie