TPS4H160-Q1: TPS4H160BQPWPRQ1 CS pin

Part Number: TPS4H160-Q1


Hi, TI team:

could you tell me the CS pin(10 pin) output voltage and current when in the fault mode? our Vvs = 11.5V.

I find the value is 4.5-6.5V in the datasheet, it is right?

image.png

 

Please check the CS pin divide resistor value, I used 510R and 1K, so when in the fault mode, CS pin voltage is 3V ~ 4.5V? my MCU pin is 3.3V, so I worry the 4.5V will damage MCU, do I need change the divide resistor to 510R and 510R? the CS pin voltage is 2.25V ~ 3.25V, it will not damage MCU pin?

image.png