Part Number: TPSM63606
Dear Specialists,
My customer is considering TPSM63606 for variable power supply with digital poteitiometer.
However, they encountered oscillation.
I would be grateful if you could advise.
---
I created a variable-output power supply by using digital poteitiometer for RFBT.
Increase output voltage causes oscillation.
Reducing RFBB increases the stable voltage range.
When RFBB=2.4kohm, output 7V stable and RFBB=1kohm, output 11V stable.
I suspect the oscillation is caused by FB loop due to the parastic capacitance of digital potentiometer.
Could you please advise three questions listed below?
(1) When add CFF between Vout and FB pin, result any improvement?
How much pF should be connected?
The digital potentiometer is used AD5291 between A pin(85pF) and W pin(65pF).
(2) Would it be advantage to put the digital potentiometer to RFBB, instead of RFBT?
(3) Would there any othe measures?
---
I appreciate your great help in advance.
Best regards,
Shinichi