Part Number: LM3644EVM
Other Parts Discussed in Thread: LM3644, USB2ANY
I can't open LM3644 GUI tool on windows 11. Tried in 3 different windows 11 installed laptops.
Is there a way to make it work?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ser,
Our expert will take a look and come back to you later soon.
Regards,
Emma Wu
Hi Ser
The LM3644 GUI does has some compatibilities issues, unfortunately this tool is old and there is no resource for the militainment .
Please let me check if there is other way to control LM3644 by USB2ANY without the LM3644 GUI.
Thanks and best regards.
Hi Ser
Sorry for late reply. Not sure if you have resolved the issue. I tested on the EVM and you can directly control LM3644 using the USB2ANY EXPLORER :
1. download the USB2ANY explorer

2. select I2C interface
3. write codes to control the LM3644. A very simple test example is that: with Vin=3.6V, write 0x01 register as 0x0B, the LED1,LED2 will light up; the torch current is as default;
Thanks and best regards.