I have integrated a TPS1H000-Q1 into our product and it works fairly well. In our application we are using it to drive an electronic load prodived by our customers. Since digital electronics can go into standby mode, open load dection isn't really a concern for us.
It would be nice if we could detect an short circuit/ over-current condition while ignoring any light load condition. Is there a way to configure the TPS1H000-Q1, or drop in a pin compatable device that can do this? Obviously one solution would be to add a 10mA load on our pcb, or sense the output voltage of the TPS1H000-Q1.