Part Number: LM8365
Other Parts Discussed in Thread: LM8364,
Dear Team
Scope : to pass Voltage dips test 10ms
I need a support for Correct brownout function ic for UCC28180D PFC controller 1000W , i tried with LM8365 reset ic based on your thread using LM8364.
Schematic added and Label Cven connected to 6 th pin of UCC28180D
Input voltage 124VAC the output should be > 2.85v at the 2nd pin of LM8365 but there is a voltage down and up .
The screenshot shows input voltage around 307V dc ( bus voltage)

The screenshot shows input voltage around 307V without Lm8365