What is the difference between TL7702A & TL7702B?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
There are various small differences, mostly insignificant, in the electrical characterization of the two parts and in the recommended operating conditions. But what I see as the only big difference between the two parts is that the RESET becomes active when Vcc ramps up to 1V for the TL7702B but does not become active till Vcc rises to 3.6V at turn-on for the TL7702A.
Regards
Bill