Part Number: TPS65262-2
Hi Team,
Please review the schematics attched for the below parameters,
VIN_LDO : 5V, LDO1_OUT : 3.3V, LDO2_OUT : NC
VIN_BUCK : 5V, BUCK1_OUT : 1.8V, BUCK1_SS : 1.2ms, BUCK2_OUT : 2.5V, BUCK3_OUT : 0.85V
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65262-2
Hi Team,
Please review the schematics attched for the below parameters,
VIN_LDO : 5V, LDO1_OUT : 3.3V, LDO2_OUT : NC
VIN_BUCK : 5V, BUCK1_OUT : 1.8V, BUCK1_SS : 1.2ms, BUCK2_OUT : 2.5V, BUCK3_OUT : 0.85V
Thanks
Hi Nachiketh,
The schematic looks fine.
Thanks
Kind Regards,
William
Hi William,
1. How to calculate the feed-forward capacitors near the outputs, Is there any formula for it?
2. Are the current feed-forward capacitors used correct?
Thanks
Hi Nachiketch,
Please check the comments below:
1. Here is the formula to calculate the feed forward capacitor
fco = cross-over frequency. It is usually switching frequency/10
R1 is the top feedback resistor.
R2 is the bottom resistor.
2. Start with 50 pf
If there any low frequency ripple in the output, you can try to increase the Cff value to reduce the ripple.
Thanks.
Best Regards,
William