Hi team,
My customer is using the TPS54620, and we are experiencing power startup failures at low temperatures. Could you please review the following?
Conditions
-
Input voltage: 14 V
-
Output voltage: 0.95 V
-
Output current: 6 A
-
Temperature range where the issue occurs: –10 °C to 5 °C
Symptom
-
PWRGD drops due to OVP
Verification
-
Changed constants on the COMP pin
-
R2440: 3.3 kohm → 1 kohm
-
C2458: 0.01 µF → 0.047 µF
-
-
Result: No symptom observed
-
Phase margin of the board at room temperature (before change): 32°
-
Phase margin after change: 66°
Our view We are concerned that excessive overall loop gain and insufficient phase margin allow load transients or switching noise to be superimposed on Vsense, causing the output to overshoot transiently. As a result, PWRGD goes outside the range of 94% Vref < PWRGD < 106% Vref, which we believe triggers the Fault condition.
Question We would like to hear TI’s view regarding this phenomenon.
Best regards,
Kyohei