Part Number: BQ41Z90
Other Parts Discussed in Thread: BQ40Z50, , BQ76952
Dear
1.Is there a difference between the IT-DZT algorithm of the bq41Z90 chip and the impedance tracking algorithm of the previous bq40z50?
2. Does the IT-DZT algorithm of the bq41Z90 chip also require matching the battery cell ID?
3. Can bq41Z90 achieve a SOC accuracy of 3% across the full temperature range.
4. Is the bq41Z90 an MCU addition based on the bq76952?
5. Has the current sensing accuracy of the bq41Z90 chip been improved upon the basis of the bq76952?
3) Other TI information.