This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61040-Q1: Absolute maximum ratings of the FB pin of the TPS61040-Q1

Part Number: TPS61040-Q1

Hello

I'm using the TPS61040-Q1 to generate 12V from 5V.
After the 5V is turned off, the 12V slowly decays, resulting in a voltage at the FB pin higher than VIN.
However, the absolute maximum rating of the FB pin is VIN + 0.3V.

Do I need any kind of protection circuitry for the FB pin?