Other Parts Discussed in Thread: BQ25770G, BQ25773
Hi everyone,
I'm using the BQ2730 on a custom board for a project we're working on. The PDF lists the max input voltage on VBUS to be 32V, and the recommended voltage to be 26V. What isn't really defined is what happens in between those two voltages.
Given that many new USB-C PD devices can outpu 28V, is the charger safe to use at this voltage, even if perhaps it's non optimal. I feel like there is some abiguity with this device, and other forum questions related to it didn't do much to help clarify it. Can you say unambiguously if using 28V as input for VBUS is acceptable please?
Thank you.