This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: Design Energy

Part Number: BQ34Z100-R2

Hello,

I had a question about the design energy parameter for the BQ34Z100-R2 fuel gauge. We are using it for a 14S1P configuration with a nominal pack voltage of 51.8V, or 3.7V nominal per cell. Which value do I use when calculating the design energy? 

Also, the current scale on the gauge is set to 10. Do I use the unscaled design capacity or the scaled design capacity when calculating design energy?

Thanks,

Jordan