Part Number: BQ25176J
Other Parts Discussed in Thread: BQ25171-Q1
Hi, I'm looking at using a BQ25176J to replace a soon to be obsolete single cell Li-ion charger which has an Enable pin. It looks like I could use the TC pin on the BQ25176J as an Enable/Disable, but holding voltage at TC between 188mV and 610mV to keep the battery charging current at the desired level looks problematic. It looks like I would have to use a Hi-Z / Active Low output to drive the pulldown resistor to make this work. Is there a recommended circuit that can do this? Thanks.