This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92613-Q1: Using TPS92613-Q1 for driving resistive load

Part Number: TPS92613-Q1
Other Parts Discussed in Thread: LM3405, TPS92200, LM3405A

Hi,

I am planning to use TPS92613-Q1 to drive a resistive load which takes 0.55A@5V.

My input voltage is from 5V adapter.

The main reason for slecting the driver is, i want to control the resitive load current using PWM pin to cotrol the heating of the resistor.

Do you see any issue with this approach.

Looking forward to your guidance.

Regards,

Rahul