This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS543C20: Requesting for alternate suggestion for TPS543C20RVFT

Part Number: TPS543C20
Other Parts Discussed in Thread: TPS546E25, , TPS546D24A

Dear Team, 

I want to know about is there any alternate part available for the following conditions.
I have 2 major Condition.

1, It has to be AEC Qualified.
2, It has to be part with -55°C to 125°C Temp support

The above mentioned condition either 1 or 2 is enough. It is not must to follow both. it should be either AEC or the mentioned temp support.

Now comes the parameter requirement.
My input voltage is 12V.
Planing output voltage is 0.85V
Current requirement is 70A to 80A (2x stackable is also fine)

Hoping for the reply from your side as soon as possible.

Thank you and best regards, 
Maharajan P