This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High-current Step-Down-converter - modular

Other Parts Discussed in Thread: TPS40055, TPS40170, TPS40140

Hi!

I am lokking for a Buck-Converter from 24V (23-28V) to 12V (adjustable 12-15V). I need to convert 24V from a lead acid battery to 12-15V. There are different loads up to 100A. So I think the best thing is a multiphase-design. I to split it into a buck-converter with about 10A (or a bit more) and to use a few of them in addiction of the load (e.g. 4 converters with load-share for a 12V/35A-load).
I found the TPS40055, TPS40170 and a few more buck controller, to do that.
What could you recommend to use? Is there any matchable design notes available?

Thanks in advance

Uwe